Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Frequency used on SmartStruxure Lite SE7000 controller Zigbee communication

Issue

Which frequency is used by the Zigbee wireless communication protocol used in the SmartStruxure Lite?

Product Line

EcoStruxure Building Expert

Environment

  • SmartStruxure Lite
  • SE7000
  • Zigbee

Cause

2 different versions of Zigbee (W and P) are used, depending on generation of product.

Resolution

 

W and P are using the same layer IEEE 802.15.4 at 2.4 GHz frequency, only the "language" is different. (they can't talk to each other)

For more information and details on the different Zigbee protocols, please see:

Tags (1)
Labels (1)
100% helpful (1/1)
Contributors