Issue
Needs to replace older actuator on DN15 valves that are still working.
Environment
Forta
V282 DN15
V294 DN15
V384 DN15
V386 DN15
V394 DN15
V298 DN15
Cause
Replacing old actuators on DN15 valves that are still in good working condition.
Resolution
For fitting of Forta actuators on DN15 valves, please use mounting kit according to this 0FL.