Issue
IAC Touchscreen passwords.
Environment
IAC
Touchscreen
600
IAC600
Cause
Customer did not know the passwords.
Resolution
The password that will allow you to read point values via the Touchscreen is 1234.
The password that will allow you to make changes to point values via the Touchscreen is 4321.
There is also a maintenance password available, but unless the operator knows the Touchscreen operation well, this should not be used. Please refer to Product Support Services if this password is required.
To view the Touchscreen User Guide, please click HERE.