Issue
After upgrading to Continuum 1.94, Cyberstation throws the following error:
Failed to call pILiveData -> GetLiveData(). ACDataServices has an error.
Product Line
Andover Continuum
Environment
- Continuum 1.94
- Schedule
- Error
Cause
This behaviour is due to a bug that was described in TPA-BOST-12-0002 00 Schedule Exception Errors.
Resolution
Install the CyberStation v1.94 SP1 - Software which can be found on the Exchange Extranet.