Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Error when opening OpenLNS Plugin in SmartStruxure

Issue

When open the OpenLNS Plugin in SmartStruxure, an error will pop up: The procedure entry point ?OnFinalRelease@xRefCountObject@@MBEXXZ could not be located in the dynamic link library LdvxShared.dll.

Environment

SmartStruxure

OpenLNS

LonMaker 3.1

Windows 7

Cause

LonMaker 3.1 is not supported in Windows 7, even though sometimes it will work. But when it works with OpenLNS plugin, it will fail.

Resolution

1. Upgrade LonMaker from version 3.1 to 3.2. Or remove LonMaker and other Echelon program in the computer. Also uninstall the OpenLNS program.

2. Try to install the OpenLNS program again. It should work now.

Tags (1)
Labels (1)
No ratings