Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Error: "Encountered an improper argument" or Microsoft .NET Framework error: "Unhandled exception has occurred..."

Issue

Errors occur when trying to open up graphics in Vista Workstation similar to these:

Microsoft .NET Framework

Unhandled exception has occurred in a component in your application. If you click Continue, the application will ignore this error and attempt to continue.

A generic error occurred in GDI+.

TAC Vista Workstation

Encountered an improper argument.

Environment

  • Windows 7
  • Windows XP
  • Vista
  • TGML

Cause

Installing Windows XP on a machine that came pre-installed with Windows 7 has been observed to cause this problem.

Resolution

Computers that are sold with Windows 7 pre-installed typically have hardware that is optimized for Windows 7 and often experience a variety of problems when they are re-imaged to Windows XP.

The best solution is to re-install Windows 7. TAC Vista 5.1.4 and newer is compatible with Windows 7 as well as some third-party LNS network tools (check manufacturer's websites for more information). Windows 7 Professional, Ultimate and Enterprise can run programs using "XP Mode". XP Mode is a separate download available for free from Microsoft's website.

Tags (1)
Labels (1)
No ratings