Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Error: NS #44 IcaErrNsBadParms

Issue

Invalid parameter values.

Product Line

TAC Vista

Environment

  • NL220
  • LonMaker
  • Vista
  • LNS

Cause

The NS #44 error is a generic, catch all error. Most likely a parameter was changed in the device template and issued a Build (or a Build and Load) instead of a Build All (or Build All and Load). It can also indicate that NodeBuilder has received a bad parameter. This error often occurs when a device template has been changed. Whenever the device template is modified, the project must be rebuilt.

Resolution

If a change is made to the domain table entry in the reset clause, this error will occur. It's not really an error in this case. NodeBuilder will issue a reset command before putting it online. If the subnet / node address changes after the reset, NodeBuilder will no longer be able to talk to the node since the subnet / node address of the node will have changed. It will be using the wrong subnet / node address.

For more information or help contact Echelon support here.

Tags (1)
Labels (1)
No ratings