Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Error Getting IIS object: IIS://LocalHost/W3SVC/1/Root/webclient. Automation error Invalid syntax when installing webclient

Issue

Error Getting IIS object: IIS://LocalHost/W3SVC/1/Root/webclient. Automation error Invalid syntax when installing webclient

Environment

Webclient

Windows XP

Windows 7

Cause

IIS must be installed prior to webclient or the webclient applications cannot be created

Resolution

1. Install IIS prior to the webclient install (See the installation guide section Pre-installation Microsoft Tasks)

2. If IIS is already installed, run the following command from a DOS prompt (Start>Run>cmd)

CD\ + enter

Cd \Windows\Microsoft.net\Framework\v2.0.50727> aspnet_regiis.exe -i + enter

Reboot the PC and reinstall webclient

Windows 7: Ensure that all the specific IIS components are selected according to the webclient installation guide

See the section Configuring IIS for Windows Vista and Windows 7. There are specific components that must be selected in order for the webclient applications to work properly. If a component was missed, select it, then restart IIS and Continuum.

Labels (1)
No ratings