Issue
Is the Personnel Import Utility (PIU) included with Continuum or is it add-on software?
Product Line
Andover Continuum
Environment
CyberStation
Cause
The PIU is sometimes confused with the Personnel Data Importer, which is add-on software.
Resolution
The Personnel Import Utility is part of the Continuum system but must be enabled in the CyberStation key before it can be used. The key must have the -D (Data Exchange) option in order for the PIU to work.