New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

- Join us on October 23rd for a live Panel session to discuss The Power of a Sustainable Ecosystem with Hervé Coureil, Chief Digital Officer of Schneider Electric and other great speakers. Register here!

Embedded WebStaion client license when logging directly into a SmartX server no longer needed

Issue

Embedded WebStation client licenses were needed when logging directly into a SmartX server as of 3.0.1 but are no longer needed

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Webstation
  • Building Operation Smartx Server

Cause

The license requirement is being removed due to market feedback. The quantity of the direct web connections to the SmartX server is restricted by the Architectural Guidelines only

Resolution

The change is available via a Hot Fix to version v3.0.3 and will be incorporated into Maintenance Release v3.0.4. In both the HotFix and the Maintenance Release, license status presentations in Device Administrator and Control Panel will indicate the availability of 99 client licenses. However, the supported quantity of direct web connections to a single SmartX server is established by the Architectural Guidelines; currently, the maximum is five concurrent connections. In v3.1, Device Administrator and Control Panel will not list client license availability at the SmartX server level since it is not constrained by licenses.

Tags (1)
Labels (1)
100% helpful (1/1)
Contributors