Issue
ETHERNET Cable Requirements.
Environment
Sigma 4.05 and earlier versions.
V53 and ARM7 Processor Boards.
Cause
ETHERNET Network cabling advice.
Resolution
The Sigma Cabling Guide should be followed when installing an ETHERNET network: Sigma Cabling Guide 2.2
Further information about cabling can be found in the following guides:
For V53 Processor Boards (UNC496, 596, UNC532, DNN and IC integration controllers): Cguide26.pdf
For ARM7 Processor Boards (UNC696, 796 & UNC632): Cguide31.pdf Cguide32.pdf
For ARM7 Processor Boards (DNN3 Decentralised Network Node): Cguide33.pdf
For ARM7 Processor Boards (IC3 Integration Controller): Cguide34.pdf
RJ45 Plug connections are: