New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements

- Who are the top users of September? Discover them here!

- Check out the ESS Active Energy Management Blog now! 

- Join us on October 23rd for a live Panel session to discuss The Power of a Sustainable Ecosystem with Hervé Coureil, Chief Digital Officer of Schneider Electric and other great speakers. Register here!

EH Series Humidity Sensors

Issue

The specifications and setup details of the EH series humidity sensors.

Product Line

Andover Continuum, EcoStruxure Building Operation, Field Devices, TAC IA Series, TAC INET, TAC Vista

Environment

Humidity Sensor

Cause

The EH Series Room, Duct and Outside humidity sensors are a universal Relative Humidity transmitter that can be powered with either a +15 to 36 Vdc or 24 Vac supply voltage. The EH series sensors are designed with a field selectable 4-20 mA, 0-5 Vdc, or 0-10 Vdc output signal that is equivalent to 0 to 100% RH. The EH Series is used in building automation system, humidity chambers, and OEM applications and is compatible with Vista, Continuum, I/Net, I/A, and SmartStruxure systems.

Resolution

EH Series Humidity Sensors

Click the below links to look at the documentation for these sensors including the dip switch settings.


Old EH Series Humidity Model

For information on the older style of dip switches (models with two separate sets of dip switches), see the document below.

Tags (3)
No ratings