Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Duplicate Cardholder when using the PIU (Personnel Import Utility)

Issue

After using the PIU there are duplicate cardholders

Product Line

Andover Continuum

Environment

  • Continuum
  • PIU
  • Windows XP
  • Windows 7
  • Windows Server 2003
  • Windows Server 2008

Cause

A unique alias must be specified with the transform or duplicate records will be created

Resolution

Each alias must be unique. Information that is updated for a personnel object will be triggered off the alias. If the alias already exists in the database, then just the new information is added. If the aliases are not unique, a new record will be created. (See “Saving a Configuration and Importing Data into CyberStation.”) To verify this, when previewing your data, make sure that every alias name under the "Alias" column is unique before importing.

See Personnel Import Utility documentation for more information

Tags (1)
Labels (1)
No ratings
Contributors