New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Does Configuration Server for an i.Lon 1000 have to be running all of the time?

Issue

Does Configuration Server for an i.Lon 1000 have to be running all of the time?

Environment

i.LON 1000

Cause

The Config Server provides the path for communication to the iLon when used as an RNI.

Resolution

If using the i.Lon 1000 as an RNI to communicate with the LonWorks network, then the Config Server must be open.  

If the i.Lon 1000 is being used as a router (not RNI), it is not necessary to have Config Server running unless you are in the configuration process for the router.

Tags (1)
Labels (1)
No ratings