Issue
Default IP address of a SmartStruxure Lite MPM
Product Line
EcoStruxure Building Expert
Environment
MPM
Cause
What is the default IP address of a SmartStruxure MPM?
Resolution
Out of the box, the default IP is 10.50.80.3 subnet mask 255.0.0.0
This should be changed to suit the project requirement.
- Log into the controller using the default IP address.
- Edit the Ethernet setting, changing the IP address, Subnet Mask and Default Gateway.
- Click save.