Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Database maintenance before performing an I/NET upgrade

Issue

When upgrading to a different revision of software in I/NET Seven, there are a few steps that are highly recommended to ensure that the database doesn't get corrupted during the upgrade.

Product Line

TAC INET

Environment

I/NET Seven

Cause

Performing an upgrade of I/NET Seven software.

Resolution

  1. Close I/NET
  2. Start DB Create and select the Verify Database option.
  3. Verify that the database has 0 differences.
  4. Select Upgrade Database to force an upgrade
  5. Select the Verify Database option again.
  6. Now back up the database to the local drive or media and proceed with the upgrade.
  7. Once completed, Select Restore database and proceed to where the back up is and restore the database to the system. 

Refer to How to Troubleshoot on DBCreate for more issues about DBCreate.

Tags (1)
Labels (1)
No ratings