New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Cyberstation randomly stops sending email notification of alarms

Issue

Webclient fails to send alarm events (using Outlook). This happens every few days.

The Windows event viewer on the IIS (Webclient) server has a few errors happening at the same time.
Errors include Continuum losing connection to the database and going into 'no database mode'. Then it restores the connection after few minutes. At almost the same time an error occurs related to 'accdataservices.exe'. Also, an error occurs indicating that Outlook has failed to communicate with the exchange server.

Environment

Webclient v1.74, v1.81, v1.82, v1.90

MS Outlook

MS Exchange

Cause

Continuum will randomly stop sending emails for alarms that are configured to send emails. Manually sending of emails from Outlook still works but CyberStation will not send out the message. There are no Outlook errors posted in the Windows Event Viewer and there are no Cyberstation error messages related to email.

Resolution

There are hotfixes, for some of the above versions, to fix this issue.  Contact Product Support Services if you need these hotfixes.

Note: Versions 1.91 and higher have the updated code. 

Tags (4)
Labels (1)
No ratings