New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Creating Critical, Priority, Routine, Transaction event pages on a 527/731

Issue

Creating Critical, Priority, Routine, Transaction event pages on a 527/731

Environment

  • Xenta Server
  • Xenta 527, 731

Cause

When using Vista to access an I/NET network you have 4 views for the Alarms and transactions. To create these views on the web with a Xenta 527 or Xenta 731 you will need to create event pages with different filters.

Resolution

  1. Add a new event page in Xbuilder and use the InetAMT filter file.
  2. Right click on the event page and select Setup Event Viewer.
  3. Click the filter icon in the top left corner and use the following guidelines for the type of page you are trying to create:
    Critical Alarms - Priority From 1 To 1
    Priority Alarms - Priority From 2 To 2
    Routine Alarms - Priority From 3 To 3
    Transactions - Tenant: *
  4. Each event page will have a different filter. To match I/NET or Vista you will need to create four pages.
Labels (1)
No ratings