New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Announcements

- Discover the Exchange Community Top members of October here!

- The member of the month: Vassil, EcoXpert Master read the article here!

Convert a Xenta 121-HP to a Xenta 121-FC

Issue

Is it possible to convert a Xenta 121-HP to a Xenta 121-FC?

Product Line

TAC Vista

Environment

Xenta 121

Cause

The hardware controller was purchased as a heat pump or fan coil unit, and the opposite is needed for the software application.

Resolution

As of August 2011, it is possible.

  1. Download the NXE file and XIF file for the desired application
  2. Download the files to the Xenta 121 using Lonmaker or NL220

This will be blocked in the future.

Tags (2)
Labels (1)
No ratings