Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Continuum runs very slowly, taking up to two minutes to first startup

Issue

Continuum runs very slowly. Taking up to two minutes to first startup. Generally opening up Continuum Explorer and any other objects are seen to be slower than normal as well.

Product Line

Andover Continuum

Environment

Continuum v1.94 and above.

Cause

There was no Security Key connected and Continuum was running in Demo mode.

Resolution

Install valid Security Key and restart Continuum.

This symptom can also be caused by a missing or corrupt driver for the Security key, see Re-install of Continuum system and security key is not being recognized for details on re-installing the Security Key driver.

Note: Want to know what features are supported in Demo mode? See How do we run Continuum in Demo mode and what features are available?.

Tags (1)
Labels (1)
No ratings
Contributors