New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Communicate with both TACNV (TANV) and SNVT in the same device

Issue

Is it possible to communicate with both TACNV (TANV) and SNVT in the same device?

Product Line

TAC Vista

Environment

  • TAC Xenta 300, TAC Xenta 401, TAC Xenta 280
  • Menta

Cause

Want to use SNVT communication for connections to Lonworks devices and TACNV (TANV) for connections to other programmable TAC Xenta controllers.

Resolution

There are no problems with this, however you need to verify that the total number of TACNV and SNVT does not exceed the limit for your type of device.

Tags (7)
Labels (1)
No ratings