Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Care should be taken when editing a script program on a working site

Issue

Care should be taken when editing an Automation Server script program in a working system

Environment

Automation Server Script program

Cause

If a script program "Numeric Input",  "Numeric Output" or "Numeric Public" line is modified, but includes a syntax error or a reserved word, then saved, the binding for this line may be broken.
As below

 After editing the Numeric Input line using a reserved word, this line bindings are broken

Resolution

Always be extra careful when modifying scripts running live plant. In this case it would be better to add a new extra "Numeric Input", "Numeric Output" or "Numeric Public" line, rather than modifying an existing one.

The binding below are not broken

NOTE This issue was fixed in v1.7

Tags (7)
Labels (1)
No ratings