Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Can the red crosses (that indicate that a signal is offline) in Vista or SmartStruxure Workstation/Webstation be disabled?

Issue

Can the red crosses (that indicate that a signal is offline) in Vista or SmartStruxure Workstation/Webstation be disabled?

Product Line

EcoStruxure Building Operation, TAC Vista

Environment

  • SmartStruxure TGML Graphics (Workstation, Webstation)
  • Vista TGML Graphics (Workstation 5.X, Webstation 5.X)

Cause

When a signal which is bound to an object in a TGML graphic is offline, this is indicated by a red cross when viewing the graphic in Vista or SmartStruxure Workstation or Webstation.

Resolution

This can easily be disabled in TGML by adding a script to the OnSignalChange event:

function signal(evt){
  evt.preventDefault();
} 

Note, this script will only disable the red X when a point is offline. This does not address any issue that might cause points to be offline.

A short video is available on this process, to review, please see SmartStruxure - Graphics - Removing Red Crosses.mp4.

Tags (5)
No ratings
Contributors