Issue
Can not get CIPCL to autostart
Environment
- TAC Vista
- Windows 2008 R2
- Windows 7
Cause
Windows will not allow modification of the registry unless the application is started with the "Run as Administrator" option.
Resolution
Right click on TAC Vista Server and choose Run as Administrator.