Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Can more than 25 browser sessions be supported by Web Client?

Issue

Over 25 user Web Clients are required

Product Line

Andover Continuum

Environment

Web Client

Cause

Web Client licenses are only available for 1 , 2, 5, 10, 15, 20, or 25 users

Resolution

Each Web Client session can support up to 25 concurrent browser sessions, for a large system that requires additional sessions additional Web Client servers can be used, each supporting up to 25 Users.

Each Web Client server however will have a different IP address / URL, so if a user finds one server fully utilized, they will then need to connect to a different server/ address to connect to the system.

Also see How to determine if SU, LAN, or WEBC security keys are required for your project for information on Licensing.

Tags (3)
Labels (1)
No ratings