Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Can Personnel Manager profiles be linked to Personnel objects

Issue

A university customer has two personnel "types" - faculty/staff and student. They would like to link a different Personnel Manager profile to each type of personnel so that when the record is edited it opens using that profile. Can this be done?

Environment

CyberStation

Personnel Manager

Cause

A university customer has two personnel "types" - faculty/staff and student. They would like to link a different Personnel Manager profile to each type of personnel so that when the record is edited it opens using that profile. Can this be done?

Resolution

Unfortunately, this is not a feature in the current (v1.93) or older CyberStation versions.

You can open the Personnel Manager and then switch to a different profile and enter the personnel data, but that profile is not linked to the saved record. So, subsequent editing of the record will open in the default (current) profile.

Tags (1)
Labels (1)
No ratings