New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

CE Declaration of Conformity Certificate for manufactured cables

Issue

CE Declaration of Conformity Certificate for manufactured cables for interconnecting EBO modules.

Product Line

EcoStruxure Building Operation

Environment

Cabling

Cause

No CE Declaration of Conformity available for the SXWSCABLE10001 and SXWSCABLE10002 that connects EcoStruxure Building Operation AS-P and IO modules when fitted for example: when modules need to be mounted on separate DIN rails.

Resolution

CE Declaration of Conformity certificate is not required for an item e.g. premanufactured interconnecting wiring that has no functionality or is inert to the operation of the system. 

Europe – CE Marking
In general, CE Marking Directives are aimed at products, not at components, although there are some exceptions. Wire and cable products are one of those exceptions that stand out. On its own, wire or cable has no defined use or application, in that it must be built into something to be useful.

Tags (1)
Labels (1)
No ratings