Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Bas 2800+ message "No Logging Databases Have Been Specified".

Issue

No Logging Databases Have Been Specified

Environment

Windows

Cause

No Logging Databases Have Been Specified.

Resolution

  1. Log on to the Bas2800+ system
  2. Open Dataview
  3. From the menu select File then New
  4. From the menu select Data then Logging database.
  5. If there is a registered database in the Registered database Window you can select this.
  6. If the Registered database window is empty, press the Add button.
  7. Select the logging database you wish to use.
    (Default database "BAS2800.DBS" is installed with the software.)
  8. Press the OK button to select the database.
  9. On the Logging database Window press the OK button to assign the logging database.
  10. The error message should disappear.
Tags (1)
Labels (2)
No ratings