New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Automation Server I/O Modules firmware

Issue

Experiencing issues with I/O modules that may include:

  • Backplane failure causing modules to assume wrong module ID
  • Input filtering problems on RTD modules
  • Stability due to electrical noise

Product Line

EcoStruxure Building Operation

Environment

  • EcoStruxure Building Operation
  • StruxureWare Building Operation
  • Automation Server I/O Modules

Cause

The latest I/O module firmware version will correct known issues while also ensuring that the system is up to date and compliant.

Resolution

The latest I/O module firmware can be located on the Exchange by searching for I/O Module firmware. Each firmware download zip file will contain a ReadMe file that explains what was corrected in that version. 

Refer to Upgrading SmartStruxure IO Module Firmware for the procedure to upgrade the I/O module firmware. 

Tags (2)
Labels (1)
50% helpful (1/2)