Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Automation Server CPU usage between 80-100%

Issue

Automation Server CPU usage goes between 80-100% even with few programs, trends or alarms.

Product Line

EcoStruxure Building Operation

Environment

AS Automation Server

Cause

Cause 1: BACnet into AS uses a lot of resources

Cause 2: The AS has bindings from a point to a variety of places

Also check out the AS CPU and Memory Loading Quick-Help video on the Exchange.

Resolution

Example Resolutions in order:

  1. The issue described is Functions as Design in StruxureWare Building Operation. The AS results with high CPU percentage with just one point from BACnet interface loaded; however, it had no effect on AS performance.
  2. Check the propagation of values. An example would be a Space Temperature which is required by the field bus, the BACnet interface, LON interface, etc. Make sure to properly disseminate this value so to avoid overloading the CPU.
Tags (1)
Labels (1)
100% helpful (1/1)
Contributors