New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Automatic Database (DCU) SAV's occurring straight after starting I/NET.

Issue

Automatic Database SAV's occurring each time I/NET is started, this is causing I/NET to become slow to respond to other actions.

Why are Automatic Database (DCU) SAV's occurring during daytime operating hours? 

Environment

I/NET Seven 2.44 and above

Cause

This is a new feature added so that the Network Functions; DCU Time Synchronization,  Automatic Database Save and Special Day Broadcast no longer require I/NET application to be running, only the InetIoSrv is required to have these features activate.  Additionally each time the InetIoSrv.exe is started and after a nominal delay (approximately 60 seconds) these are also all activated.

Resolution

At this time there is no mechanism to stop these initial features from activating each time the InetIoSrv.exe is started.  If you are starting the InetIoSrv on multiple or regular occasions it may be best to either disable these Network Functions (in particular the Automatic Database SAV) during this time or ensure that the SAV files are all current in the nominated SAV directory as defined in the active Configuration Profile.

Tags (1)
Labels (1)
No ratings