New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Assa Abloy Continuum Integration

Issue

If using the Assa Abloy Integration for a Wireless Lock interface and pairing locks on Hub 11, only lock one is able to be paired at address 1 and functions correctly with older versions of software. No more locks can be paired after that although the Hub itself is able to handle more than one.

Product Line

Andover Continuum

Environment

Continuum Version 1.94 and above

Cause

The version of software that is used for the application needs to be the latest version as compared to the older version 2.1.7. When this version is used the Hub only allows one lock to be paired although it is set for Multiple Lock Configuration.

Resolution

When purchasing the applicable hardware from Assa Abloy, ensure that the version that is being sent out is the latest 10.2.28619.

Tags (1)
Labels (1)
No ratings