Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Are there I/A Series R2 and G3 objects for interface with the SE7000 Series Room Controllers?

Issue


Are there I/A Series R2 and G3 objects for interface with the SE7000 Series Room Controllers?

Environment

I/A Series R2 and G3, SE7000 Series Room Controller

Cause

Not able to locate shadow objects with matching LonWorks program IDs within the existing I/A Series R2 and G3 modules.

Resolution

A set of new modules have been generated for use with the new SE7000 Series Room Controllers.  The new objects interface with the following program IDs.

R2 objects:

Se7273         (80:00:10:55:00:04:04:20)
Se76Pir         (80:00:10:55:00:04:04:21)
Se76RhPir    (80:00:10:55:00:04:04:22)

Click to download ... lonSchneider-2.301.330.zip
Click to download ... lonSchneider-2.301.431.zip
Click to download ... lonSchneider-2.301.534.zip

G3 objects:

Se72_73.lnml (80:00:10:55:00:04:04:20)
Se76Pir.lnml (80:00:10:55:00:04:04:21)
Se76RhPir.lnml (80:00:10:55:00:04:04:22)

Click to download ... lonSchneider-3.5.39.1.zip
Click to download ... lonSchneider-3.7.17.zip

The 3.5.39.1 module should be used with G3 versions 3.5 and lower.
The 3.7.17 module should be used with G3 versions 3.6 and higher.

Tags (2)
No ratings