New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Alarm block limitation in a single Menta application

Issue

Generating a Menta application results in the following error if the maximum number of Menta blocks is exceeded in the application:

TAM32
The maximum number of Alarm blocks is exceeded in the application.
The problem must be solved before the application can be generated.

Environment

  • Menta
  • Xenta programmable controllers
  • Xenta 281, 282, 283, 301, 302, 401, 401:B

Cause

Generating a Menta application results in an error if the maximum number of Menta blocks is exceeded in the application.

Resolution

There can be no more than 127 alarm blocks in a Menta application.

Tags (4)
Labels (1)
No ratings