Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Adding Webstation to an Existing Network

Issue

After purchasing Webstation for a site, it still will not work even though the license is being read by LM Tools

Product Line

TAC Vista

Environment

  • Vista 5
  • Webstation
  • Licensing
  • LM Tools

Cause

When adding Webstation to an existing network it important to know if this was a Vista 5 "Stand-Alone" license or a "Full" version. Stand-Alone Vista will not allow any connectivity via IP. The needed license feature that comes in the Full version is "Vista.Server.Network". This can be verified by opening the site license in a text editor such as Notepad.

Resolution

Upgrade the site to a Full Vista license that contains the needed Vista.Server.Network feature. This will allow the Webstation to connect to Vista Server. A Demo license can be used in the interim until a Vista Upgrade License can be purchased, entitled and installed on the site. More information can be found in The Vista.Server.WebApps.Access license is missing.

Tags (1)
Labels (1)
No ratings