Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Actuators - What is the replacement for the EM52L actuator?

Issue

Is there a replacement for the EM52L actuator?

Environment

EM52L actuator 8522221010

Cause

The EM52L actuator is obsolete.

Resolution

Both the EM52L actuator and the V354/V355 valves that are associated with it are obsolete, so both will need replacing.

The replacements would be the MZ20A (Selectable control signal) or the MZ20A-R (Fixed 0-10v control) actuator, with the VZ*19 range of valves.

For a data sheet for the MZ20A actuator, please click HERE.

For a data sheet for the VZ*19 valve range, please click HERE.


 

Tags (1)
Labels (1)
No ratings