Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Accommodation and Booking features in Security Expert

Issue

Security Expert refers to both Accommodation and Booking features in its Client which would suggest that it is currently capable of handling the Booking/Accommodation of Users as well as controlling their Access, but this is not the case.

Product Line

Security Expert

Environment

Security Expert

Cause

Security Expert has an Accommodation Tab in the User Menu of the Client, which seems to suggest that Rooms can be booked in the system.

Accommodation.png

A Booking System option is also found in the Licensing Menu, which would suggest that Booking features can be enabled upon request.

Booking.png

Resolution

Both the Accommodation and Booking features are not currently activated however have been included in the GUI and license structure for potential 'future development'. There are no dates for when this will occur.

Tags (1)
Labels (1)
No ratings