Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Access Expert Sub-Device Integration

Issue

Unable to connect Continuum I/O's to Access Expert

Product Line

Access Expert

Environment

Win 8.1 and above on Version 3

Cause

The Continuum Integration has only been configured to bring in the AC-1 and AC-1 Plus door controllers as sub-devices.

Resolution

There is no resolution, but the Continuum I/O's are simply not compatible with Access Expert. Use Mercury 16 In/Out boards for applications that require these types of devices.

Labels (1)
No ratings
Contributors