Issue
ARCNET LAN Maximum Impedance and Maximum Distance.
Environment
Sigma all versions using ARCNET.
Cause
Advice only.
Resolution
The maximum impedance of an ARCNET LAN should be less than 100ohms.
Maximum distance for an ARCNET LAN at 156K baud rate is 800metres using the preferred cable Belden 8762, this will have a resistance of 25ohms.
For further information regarding baud rates, cable types, distance and installation guidelines please go to: Cabling Guide 2.2.