Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

A "Save Error" message that says "Not enough quota is available to process this command" is displayed when trying to save graphics.

Issue

A "Save Error" message that says "Not enough quota is available to process this command" is displayed when trying to save graphics. 

Environment

SmartStruxure Workstation 

Cause

The error message indicates that there not enough virtual memory (VM) available. 

Resolution

Close some applications and try again. If the error message is still being displayed, try increasing the virtual PC’s memory.

Windows XP:
1. Open “Control Panel” and click on “Systems”
2. Select the “Advanced” tab
3. Under the “Performance” header, click on the “Settings” button and then “Advanced” tab.
4. Click on the “Change” button under “Virtual memory”
5. Increase the size of the virtual memory and click OK to save.

Since Virtual Memory is dynamic in Windows 7, this error message is not common to a Windows 7 operating system. However, if running a lot of apps or the system has minimum requirement, it is possible that you can see it here. The following are steps to increase the VM for Windows 7.

Windows 7:
1. Open Control Panel and click on Systems
2. Select the “Advance systems settings”
3. Under the “Performance” header, click on the “Settings” button and then “Advanced” tab.
4. Click on the “Change” button under “Virtual memory”
5. Increase the size of the virtual memory and click OK to save.

VM uses the hard drive for storage.
 

Tags (1)
Labels (1)
No ratings