Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

125 kHz cards technology supported by Security Expert readers

Issue

What type(s) of 125 kHz proximity cards are supported by Security Expert Card Readers?

How to configure Secure Expert to read an Indala card (125 kHz)?

Product Line

Security Expert

Environment

Security Expert Smart Card Reader

Cause

Card readers work by modulating the electromagnetic wave in different ways to resolve between 1s and 0s. There are several different ways to bring card data across 125 kHz; ASK, FSK and PSK.

ASK : Amplitude Shift Keying
FSK : Frequency Shift Keying
PSK : Phase Shift Keying

Since the technology used is determined at the hardware level,  a reader would need to have the hardware to read a specific type.


Security Expert 125 kHz readers make use of FSK only, which means that e.g. Indala cards (125 kHz PSK technology) will not work with them.

Resolution

Use FSK technology 125 kHz cards with Security Expert Smart Card Readers.

Tags (1)
Labels (1)
100% helpful (1/1)