Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

121 controller when setup for 2 pipe system will not heat or cool

Issue

A Xenta 121-FC controller setup as a 2 pipe system will not heat or cool even though the terminal load is showing a demand.

Product Line

TAC Vista

Environment

Xenta 121-FC

Cause

The Xenta 121-FC does not have a water temperature sensor wired into the device

Resolution

For this functionality to work automatically, a water temperature sensor must be wired into the U1 terminal on the FC-121.

The other alternative is to set the supply temperature via the SNVT nviSourceTemp. This can be done from a supervisory system that is feeding the water to the 121-FC.

To use the SNVT nviSourceTemp as a solution the correct heartbeat will be require to be set in the 121-FC.

Values sent from a Xenta 121 FC/HP via SNVT bindings are not making it to the receiving controller is a link on how to set that up. 

Tags (1)
Labels (1)
No ratings