43367members
217836posts

Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Highlighted

Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Looking for options to achieve non-intrusive and near-zero latency cybersecurity of my petrochemical customer's plant industrial communications 

5 REPLIES 5
Highlighted
Ensign

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Hi,

 

Enigmedia is specialized in securing communications with two main benefits: Non-intrusive installation and near zero latency. With Mercury you can get a secure communication using a somehow unsecure medium, even if the client or access point gets compromised by an attacker the data on air will be protected with encryption (impossible to recover or modify the original data), authentication (impossible to act as a rogue device), and accounting (traceability of activities).

 

Additionally, Mercury is completely transparent to the network and compatible with any device or protocol used in the network. Thanks to that, it does not require changing, or modifying, any existing IP configuration.

 

You can find more information about Mercury in the Exchange shop in this link.

 

Feel free to reach us for more information at contact@enigmediasecurity.com

 

Best,

Highlighted

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Cybersecurity needs a holistic view. If you are looking for a technology solution and not service, you could explore the following 5 options. They are listed inside the shop (right here on exchange): 

 

1/ Claroty: https://shop.exchange.se.com/apps/38661/claroty-platform#!overview 

 

2/ Waterfall security: https://shop.exchange.se.com/apps/39811/unidirectional-security-gateways#!overview 

 

3/ Extreme Networks: https://shop.exchange.se.com/apps/39231/extremecontrol#!overview 

 

4/ Tripwire: https://shop.exchange.se.com/apps/39621/tripwire-ics-security-suite#!overview

 

5/ Indegy: https://shop.exchange.se.com/apps/41315/indegy-industrial-cyber-security-suite#!overview 

 

 

Additionally, you could also explore the best practices at:

https://shop.exchange.se.com/apps/40125/reduce-vulnerability-to-cyber-attacks#!overview 

 

Hope it helps. Inbox me your specific requirements for a customized solution to your customer needs. 

Highlighted

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Thanks. Lets take our discussion privately. I will inbox you. 

Highlighted

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Thank you for your response on options and best practices. I am sending you a message directly. 

Highlighted
Ensign

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Hi,

 

Based on our direct message exchanges, thanks for accepting our product as solution to your customer needs,

 

Thanks and regards,