Hello,
Quantum safety CPUs are not supported in the newest versions of Unity and Control Expert.
Latest supported version was Unity XLS V7.0.
Is this version compatible with Windows 10?
If it's not the case, which solutions can be used to go on programming these PLCs?
Virtual machine with Windows 7?
Best regards,
Samuel
Solved! Go to Solution.
@Slegrix Yes you right, you can only use Unity XLS 7.0 for Quantum Safety. but this is not compatible with Win 8 or Win 10.
here is compatibility matrix:
source of image: https://www.se.com/ww/en/faqs/FA342365/
the only option is using VM
@Slegrix Yes you right, you can only use Unity XLS 7.0 for Quantum Safety. but this is not compatible with Win 8 or Win 10.
here is compatibility matrix:
source of image: https://www.se.com/ww/en/faqs/FA342365/
the only option is using VM
Thank you! 👍
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!