New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Industry Automation and Control Forum
This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Highlighted
Cadet

UNITY XLS V7.0 compatibility with Windows 10 ?

Hello,

 

Quantum safety CPUs are not supported in the newest versions of Unity and Control Expert.

Latest supported version was Unity XLS V7.0.

 

Is this version compatible with Windows 10?

 

If it's not the case, which solutions can be used to go on programming these PLCs?

Virtual machine with Windows 7?

 

Best regards,

Samuel

2 REPLIES 2
Lieutenant JG

Re: UNITY XLS V7.0 compatibility with Windows 10 ?

@Slegrix Yes you right, you can only use Unity XLS 7.0 for Quantum Safety. but this is not compatible with Win 8 or Win 10.

here is compatibility matrix:

 

image.png

source of image: https://www.se.com/ww/en/faqs/FA342365/

 

 

the only option is using VM 

Cadet

Re: UNITY XLS V7.0 compatibility with Windows 10 ?

Thank you! 👍