Discuss challenges in energy and automation with a global network of peers.

39877members
181208posts

To clear and put M580 CPU to NO CONF state

Lieutenant JG

To clear and put M580 CPU to NO CONF state

Resolution – To clear and put M580 CPU to NO CONF state

For M580, there are two ways to clean the application &configuration:

  • Try to download an application, and before the downloading finish plug-out the USB.
    1. Can use Unity Loader to transfer .STU file, or
    2. Use Unity Pro XL software for transferring.
  • Using Unity function PLC --> Project Backup --> Backup Clear
  • for point 1 you can also use Unity loader

The above result will make M580 CPU into NO CONF state.

 

Transfer application by using SD-card

Required a good working M580 CPU. Insert the Schneider SD-card into the CPU and download the application into the SD-card. New downloaded application will be saved into the Schneider SD-card.

Use this SD-card and insert into the troubled CPU and power ON it. The application will be recovered and transferred into the RAM of the M580 CPU.

Michael Chan Kum Yuen
1 REPLY 1
Lieutenant JG

To clear and put M580 CPU to NO CONF state

Resolution – To clear and put M580 CPU to NO CONF state

For M580, there are two ways to clean the application &configuration:

  • Try to download an application, and before the downloading finish plug-out the USB.
    1. Can use Unity Loader to transfer .STU file, or
    2. Use Unity Pro XL software for transferring.
  • Using Unity function PLC --> Project Backup --> Backup Clear
  • for point 1 you can also use Unity loader

The above result will make M580 CPU into NO CONF state.

 

Transfer application by using SD-card

Required a good working M580 CPU. Insert the Schneider SD-card into the CPU and download the application into the SD-card. New downloaded application will be saved into the Schneider SD-card.

Use this SD-card and insert into the troubled CPU and power ON it. The application will be recovered and transferred into the RAM of the M580 CPU.

Michael Chan Kum Yuen
Highlighted
Administrator
Reply
Loading...

Re: To clear and put M580 CPU to NO CONF state

Very interesting! Thanks for sharing @Michael_Chan 

 

 

Oma
Exchange SE Global Community Manager
Community user guide  |   FAQ