AVEVA Plant SCADA Forum
A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2019-04-24 11:47 PM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2019-04-30 02:16 PM
Hi FENFEO,
I cannot speak directly for the features of EcoStruxure Machine SCADA as I lack knowledge of this offer, but I do know about EcoStruxure Geo SCADA Expert (ClearSCADA) and I think I can decipher some of the differences. The first part is that Geo SCADA is designed for wide area infrastructure such as water & wastewater distribution and networks along with upstream and mid stream oil and gas and electrical utility infrastructure where remote asset management, monitoring and control is required typically from a central control room. Geo SCADA supports protocols designed to communicate over long distances (wide area) which typically can be 10s to 100s of kms. EcoSruxure Machine would be suited for local area infrastructure or LAN - local area networks which is within the parameters of a plant where the lcoal SCADA is 10s to 100s of metres max from the SCADA. In summary: Globally EcoStruxure Geo SCADA is used in WWW, O&G and Electrical Utilities, is designed for WAN and supports protocols such as DNP3, IEC61850, IEC60870 which are exeception based protocols. EcoStruxure Machine would be designed for LAN and is suitable for OEMs / Machine builders with protocols such as Modbus. I have included some files where you can check to see some of the differentiation
EcoStruxure Machine SCADA link
https://www.schneider-electric.com/en/download/document/998-19784369_US/
Attached is the EcoStruxure Geo SCADA Expert digital brochure
Hope ths addresses your question. Thanks
Kind Regards
Craig Scott
Technical Offer Consultant - Telemetry & Remote SCADA
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2019-05-01 01:35 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2019-06-13 12:57 AM
EcoStruxure Machine SCADA Expert (formerly known as Vijeo XL), is a lite SCADA SW dedicated to machine line management and lite supervision, mainly commenrcialized in bundle with our Magelis iPCs and HMIGTU Open boxes.
I add to the answer a brochure of this SW, highligting the main features of this SW and the values of the HW+SW bundle:
- ready to use (SW tested and validated with the above mentioned HWs)
- unique point of contact for support of HW, SW and OS
- sustainable supply and compatibility in case of SW or HW evolution
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.