Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Integrate Foundation Fieldbus field devices to EcoStruxure solutions for Oil&Gas
Industry 4.0 Blog
This blog is addressing the Industry 4.0 and includes news and information aroud topics as smart manufacturing, artificial intelligence and Industrial Internet of Things (IIoT).
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results for
Show only
|
Search instead for
Did you mean:
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2019-11-0803:49 AM
Integrate Foundation Fieldbus field devices to EcoStruxure solutions for Oil&Gas
Originally published on Industry 4.0 Blog by SoftingSIA | November 08, 2019 12:49 PM
Softing, as the recognized leader in FOUNDATION fieldbus technology, presents the FG-200 gateway:
Designed for mapping the Modbus communication protocol to FOUNDATION fieldbus, Softing‘s FG-200 gateway offers the possibility to renew and expand legacy plants in the process industry by modern and highly functional segments without requiring substantial changes to the main installation. Therefore, plant operators can use state-of-the-art technology to increase production capacity while saving costs, protecting their investments, and making optimum use of the achievable lifetime of their installations.
Technical Features:
Integrate up to four FOUNDATION™ Fieldbus (FF) H1 segments (each for max. 16 field devices) into control systems supporting Modbus TCP.
The FG-200 provides device redundancy (D-3 according to FF-593) for avoiding the cost of downtime that can be substantial and may quickly run into the millions for a large plant in the process industry.
Suitable for use in hazardous areas (cULus: Class 1, Division 2, Groups A, B, C, D, IECEx: Ex nA [ic] IIC T4 Gc, ATEX: II 3G nA [ic] IIC T4 Gc), it offers intrinsically safe device segments.
FF Configuration Tool for configuration of devices and cyclic communication included.
Support of Field Device Tool (FDT) frame applications for central field device parameterization, comprehensive diagnostics or Asset Management.