43197members
217463posts

OFS to Movicon NeXt Via OPC UA

Highlighted
Crewman
Crewman

OFS to Movicon NeXt Via OPC UA

Hi everyone,

     I am Using Movicon next as a SCADA Software. My site located in a remote area. I need to connect OFS with Movicon Next via OPC UA. To do that What are the things needed to be installed on the site and which are the Ports to be Forwarded at the site firewall?

 

Regards

kpr

Tags (3)
4 REPLIES 4
Highlighted
Administrator

Re: OFS to Movicon NeXt Via OPC UA

@sbeadle , can you help here?

 

Highlighted
Commander

Re: OFS to Movicon NeXt Via OPC UA

you need to install at site:

OFS with driver you need. 

and OPC UA option checked.

 

port for firewall 48400 

 

 

there is also FAQ for this question.

FAQ 

Highlighted
Crewman
Crewman

Re: OFS to Movicon NeXt Via OPC UA

Thank you for your response,

     I'm going to connect OFS OPC with Movicon next(SCADA Software). Whether You tried with movicon or any other third party SCADA Software?.

Tags (2)
Highlighted
Crewman
Crewman

Re: OFS to Movicon NeXt Via OPC UA

Hi, while trying to connect ofs opc with Movicon next , i'm getting bad certificate Host Name Invalid error. How can rectify this issue?.

 

Regards,

Praveenraj.k