43451members
218007posts

ModBusTCPClient and ModBusTCPPortM Control Function Blocks for ModBus Explicit Communications

Highlighted
Cadet

ModBusTCPClient and ModBusTCPPortM Control Function Blocks for ModBus Explicit Communications

This document describes How to Use ModBusTCPClient and ModBusTCPPortM for Modbus Communication in M580 Standalone and Hotstandby. in EcoStruxure Control Expert ( Unity). 
Advantages:
1. Online Client Addition
2. No dependency on position of Client and port block in MAST section
3. Leveraging Simultaneous Read and Write function of Modbus

1 REPLY 1
Administrator

Re: ModBusTCPClient and ModBusTCPPortM Control Function Blocks for ModBus Explicit Communications

thanks @Rahul_S for the sharing!